Hello,
I plan on using the MAX2830 for a custom TX/RX pair for wireless audio applications, but im concerned if the chip can accept 0-20kHz on its TX pins. Does anyone with experience using this chip know if I can feed low frequency analog into it?
MAX2830
Production
The MAX2830 direct conversion, zero-IF, RF transceiver is designed specifically for 2.4GHz to 2.5GHz 802.11g/b WLAN applications. The MAX2830 completely...
Datasheet
MAX2830 on Analog.com
Hello,
I plan on using the MAX2830 for a custom TX/RX pair for wireless audio applications, but im concerned if the chip can accept 0-20kHz on its TX pins. Does anyone with experience using this chip know if I can feed low frequency analog into it?
JoeAS Do the outputs on the antenna pins not reflect direct up conversions of the TX inputs? I was told for DSBSC to have my differential audio tied into the I pins and have the Q pins connected to ground, do you think this will cause the aforementioned distortions?
JoeAS Do the outputs on the antenna pins not reflect direct up conversions of the TX inputs? I was told for DSBSC to have my differential audio tied into the I pins and have the Q pins connected to ground, do you think this will cause the aforementioned distortions?