I am using a AD 8302 to detect the phase difference between two voltage signals. The frequency is 225 kHz. I used the application notes on the topics of the AD 8302 to pick relevant input high pass filter and Cflt capacitors.
No mater what values of input and Cflt values I try, however, I get a small slope offset like in the graph shown here.
My circuit is here.
Based on the data sheets, it seams like I should not have to mess with the R110 (presently shunted) and R111(presently open) if I just want 1.8volts per 180 degrees.