I am designing an FSK receiver using the MAX41473, and I need its frequency to be very accurate. I have selected a 19.2 MHz TCXO, which feeds the XTAL1 pin (pin 9), as the datasheet mentions that the pin can be driven single-ended. The XTAL2 pin is not connected. The TCXO has a clipped sine wave output at 800 mVp-p, but my tests show that the MAX41473 does not operate properly with this signal. I have tried lowering the supply voltage from the intended 3.3V down to the minimum of 1.8V, but this did not remedy the situation. I would like to know the signal requirements of the receiver IC so that I can condition the TCXO output properly. The datasheet does not provide this information. Thank you.