Post Go back to editing

Beat Frequency in HMC6350 System

Thread Summary

The user is experiencing a 40 kHz signal at the receiver end of the HMC6350 system when no signal is input at the transmitter. The final answer suggests providing a common reference clock to both the transmitter and receiver to determine if the issue is due to clock frequency deviation.
AI Generated Content
Category: Hardware
Product Number: HMC6300

Hi, I am currently using the baseband transmission in the HMC6350 system.

When no signal is input at the HMC6300 transmitter end, the receiver end still receives a signal around 40 kHz (as shown in the figure). Is this signal caused by beat frequency resulting from a clock frequency deviation between the transmitter and receiver ends? Is there a solution for this?

Edit Notes

Add another image
[edited by: 123456qw at 6:37 AM (GMT -5) on 17 Dec 2025]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.