Hello,
I am writing this question because I have a query regarding the HMC3716LP4E phase detector and the ‘Lock Detect’ pin.
I have a PLO-based system for locking frequencies of 10-20GHz in which I use the HMC3716LP4E phase detector. I have no problems with the system itself, as it locks to all the frequencies I need and everything works properly. The problem arises because I need to lock onto extremely fast times (less than 500 ns) and to ensure that I am properly locked and meeting those times, I use the lock detect signal and the oscilloscope. This signal shows how it goes from being locked to a frequency to then unlocking and relocking, but I have a problem with it.
Below is an image showing how I analyse the signal and how the lock detect is represented. The image shows a signal at the top (channel 1) which is our trigger from an FPGA where we tell it to change the input frequency to the PLO. The signal below (channel 2) corresponds to the lock detect, which shows how it goes from being locked (5V) to unlocked (when the frequency change occurs, the signal drops below 5V) and how it recovers until it is locked again (recovering to 5V).The problem, if you can see it, is that the lock detect signal, which is represented on the oscilloscope at 500 mV per division, does not drop completely to zero. It goes from 5V to 3.5V or slightly less, and then recovers but does not drop directly to zero.
I want to emphasise that I do not think it is because of the high locking speed that it does not drop to zero, because when I looked at the lock detect signal separately, I saw that when it was locked, it was at 5V without any problem, and when it unlocked, it did not drop completely to zero, but remained at 0.6 or 0.7V, but did not drop completely to zero.
On the phase detector pin, I only have the pull-up with the 1K resistor as specified in the datasheet, so I would like to know if anyone knows what is causing this behaviour in the HMC3716, whether it is something inherent to the component or a malfunction, and how to fix it.
I also have some difficulty interpreting my signal when it can be considered that the signal is locked in such a short time, so I would like to know when the lock detect signal can be considered locked, whether when it fully recovers to 5V or when it has recovered to 50% of the rise or something similar.
Thank you,
Best regards.
Marcos.