Post Go back to editing

ADF4356 output signal issue

Category: Software
Product Number: ADF4356
Software Version: Analog Devices ADF4356 Evaluation Board Control Software v1.4.4 - April2018

When testing with the official EV-ADF4356SD development board, I observed the following phenomenon:

After starting the backend software, with the default configuration, I modified the VCO output frequency to 4915.20 MHz.

Initialization completed. The output waveform appears normal when observed with a spectrum analyzer.

The VCO output is modified to 4915.25 MHz, meaning the frequency point has been increased by 50 kHz.

After initialization, when observing the output with a spectrum analyzer, a 50 kHz harmonic with strong amplitude is visible.

As shown in the marker 2Δ1 in the figure below.

This phenomenon occurs within ±1 MHz when the VCO output is an integer multiple of the reference frequency (122.88 MHz). It disappears when the frequency offset exceeds ±2 MHz.

For example:

  • The phenomenon is observed when VCOout = 39 × 122.88 MHz ± 1 MHz.

  • The phenomenon disappears when VCOout = 39 × 122.88 MHz ± 2 MHz or beyond.


What could be the cause of this issue, and how can it be avoided?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.