Post Go back to editing

Output impedance ADA8282 - Interface to AAF LTC6603

Category: Hardware
Product Number: ADA8282

Hi! I am designing a PCB in which we plan to interface an ADA8282 with two AAFs LTC6603. The datasheet of the LTC6603 states that its input signals driver should display an output impedance lower than 100 ohms. Nevertheless, the datasheet of the ADA8282 makes no reference to its output impedance, so there is no way to know if these two componentes are a good match. 

Does anyone have any insights on the topic?

Sincerely, 

Iñaki

Parents Reply Children
No Data