Post Go back to editing

Active Bias controller issue with HMC633LC4

Category: Hardware
Product Number: HMC981LP3E

HI ADI Team!

I am using HMC633LC4 and using HMC981LP3E for Bias control!

I have both amplifier and biasing circuit on board! I am only validating the ABC part! When I measure the VGATE its 2.3V and VNEG is -2.468V and VDRAIN is 6V. The R1, R2, R4, R5, R6 and R7 are not populated on my board and they are open! 

I want to know why I am getting VGATE as positive voltage instead of Negative.

Should I Connect load(HMC633LC4) and test?

I have followed the application circuitry! 

RSense Resistor is 180R

I have used Cpout circuitry from Datasheet

SW is connected to VDIG

Enable is connected to VDIG

I am reading 3.3V from TRIGOUT

Thanks and Regards,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.