Post Go back to editing

want clarity on the impedance of the RF and LO inputs.

Thread Summary

The user wants to drive an LVDS oscillator signal into the LO of a mixer with a 50 ohm differential input. The eval board uses 50 ohm traces, suitable for single-ended drive. For differential LVDS drive, a 2:1 balun or ac-coupling one side of the LVDS signal to LOIP and LOIN to ground is recommended.

View FAQ
AI Generated Content
Category: Hardware
Product Number: ADL5801

I want to drive a signal based on an LVDS oscillator into the LO of this mixer.  The data sheet says 50 ohms differential in text and when it talks about the inputs it says they are 50 ohms.  The eval board seems to have traces for 50 ohms to ground.  So, is this 100 ohms differential (so I can drive directly into the differential input) or is it 50 ohms and I need a 2:1 impedance matching transformer?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.