Post Go back to editing

Fault: No connection to EVB

Thread Summary

The user is experiencing issues with the EVAL-SDP-CS1Z and EV-ADF4377SD1Z evaluation boards, where the software shows 'No Daughterboard Detected' despite a USB connection and correct power supply. The support engineer suspects a blank or corrupted EEPROM or issues with the I2C line. The user confirmed the 120-pin connector is seated correctly, the power supply polarity is correct, and the LEDs on both boards are lit. The user provided a log file and requested remote support due to project stress.
AI Generated Content
Category: Software
Product Number: EV-ADF4377SD1Z
Software Version: ACE 1.30.3369.1491 and board.adf4377.1.2022.16300.acezip

Hi
I am working with EVBs :
EVAL-SDP-CS1Z
EV-ADF4377SD1Z
But I don't have a connection as far as I understand I should see a connection when I see the software - green light and the component status is available
I attached the file board.adf4377.1.2022.16300.acezip to PLUG-IN
I have a USB connection I see it in the device manager
What else do I need to do to make it work I am using UG-2050 but without success
I attached a picture

I would appreciate a quick answer.

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.