KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
ADF4356
Recommended for New Designs
The ADF4356 allows implementation of fractional-N or integer-N phase-locked loop (PLL) frequency synthesizers when used with an external loop filter and...
Datasheet
ADF4356 on Analog.com
Hello,
I am currently evaluating the EVAL-ADF4356 board.
When I power up the evaluation board at room temperature and execute "Write Init. Seq", the output waveform is normal and the PLL indicates Lock.
However, when I power up the board in a –15°C environment and perform "Write Init. Seq", the output waveform shows increased noise and the PLL becomes unlocked.
During this test, the PC controlling the evaluation board remains at room temperature.
To suppress this issue, I manually wrote the VCOCORE, band, and bias values that were read at room temperature, and this completely resolved the problem.
From this observation, I suspect that VCO band selection is not functioning correctly at low temperatures.
Even when I set VCO Band Div = 255 and ADC Clock = 255 in the evaluation board GUI, the frequency of occurrence decreased but the problem was not fully resolved.
Could you please advise if there are any other possible countermeasures or settings I could try?
The setup consists of the evaluation board connected to a PC using the GUI.
The PFD frequency is below 75 MHz.
I have already checked and tried the suggestions from the following discussions, but they did not resolve the issue:
I also have ADIsimPLL and GUI configuration data available, but since they contain proprietary information, I cannot share them in an open community.
Thank you very much for your support and advice.
Best regards
Hello ambugua.
I'm waiting for a response from faikyaman.
Best Regards.
Hi,
Just for record, this is being responded to through email chain external to EngineerZone. When a conclusion has been reached, we can paste the answer to this thread.
Kieran