Hi,
I would like to use the HMC851 with a Vr between -1.5 V and -1.2 V.
Could this component fail under these conditions ?
I noticed increased thermal dispersion below -1.2 V, but this is not an issue for my application.
Thanks !
HMC851
Recommended for New Designs
The HMC851LC3C is a XOR/XNOR gate function designed to support data transmission rates of up to 28 Gbps, and clock frequencies as high as 28 GHz. The HMC851LC3C...
Datasheet
HMC851 on Analog.com
Hi,
I would like to use the HMC851 with a Vr between -1.5 V and -1.2 V.
Could this component fail under these conditions ?
I noticed increased thermal dispersion below -1.2 V, but this is not an issue for my application.
Thanks !
I had a look in our archives and was not able to find any data with the VR voltage taken below -1.2V. I see a plot in the datasheet showing output differential voltage vs VR and temperature. Notice that the cold trace is heading south at a fairly steep rate and the hot trace is also starting to deviate. That would concern me a bit, even if you don't plan to use the part at cold or hot.
So I'm not saying that you can't do this but I would say that we don't recommend it based on the little bit of information that we have.
Would you consider instead setting VR in-range and putting some attenuation at the output to get the level that you want?
I've not heard back from you and will assume that you do not need additional assistance.
Thank you for your response. However, we do not have the option to add additional attenuation at the output. The fact that the power variation changes with temperature is not an issue for us, as we have a calibration mechanism in place. Our only concern is about the reliability of this component when operating at a lower voltage, which still remains within the maximum ratings.