Post Go back to editing

Phase coherence with multiple MAX2771 front-ends

Thread Summary

The user is trying to achieve phase-coherent operation with multiple MAX2771 GNSS front-end chips. The final answer suggests setting the R divider to 1 and using a common reference with equal PCB trace lengths to all devices, or calibrating phase differences in the digital domain. The internal PLL phase behavior is not deterministic after reset and lock, and there is no way to slave other MAX2771s off a master or drive them from an external LO.
AI Generated Content
Category: Hardware
Product Number: MAX2771

I’m using multiple MAX2771 GNSS front-end chips (e.g., 4 channels) and trying to achieve phase-coherent operation.
Even if all devices share the same reference and LO, each internal PLL may lock at a slightly different time, leading to random initial phase offsets.

How can phase calibration be performed in this case?
Is it possible to feed several MAX2771 devices from an external PLL (bypassing internal PLLs) to ensure deterministic phase behavior?
Or is the MAX2771’s internal PLL phase behavior deterministic after reset and lock?

Any design guidance or examples for coherent multi-MAX2771 setups would be very helpful.

  • My guess is that you cannot do multi-chip sync. Also, I don't think that you can drive multiple devices from a single PLL. But I do need to check into this more and will get back to you once I know more. 

  • I talked to some other colleagues about this question and got a few possibilities back. Firstly because the PLL is integrated, there is no way to slave other MAX2771s off of a master. Also, it's not possible, the run one or multiple MAX2771 devices from an external LO.

    One idea that has not been tried but which may work would be to set the R divider to 1 and drive all of the MAX2771s from a common reference with equal PCB trace lines to all devices. If the R divider is at one, then you know that the external reference signal is going straight through to the phase comparator with not phase flips or start up uncertainty. So if the “R” input to all of the phase comparators is the same, I think that the output should also be phase aligned. However, we have not bench tested this.

    The other idea suggested was to calibrate out the phase differences. So you would again run all devices from the same reference but might be setting the R divider to a value other than one. Then you would digitize the samples from the multiple MAX2771 devices and figure out the phase difference (with all MAX2771s driven by a common reference clock and a common RF signal. Figure out how much phase shift you have from channel to channel and correct in the digital domain. 

    For both scenarios above, you would need to verify whether the phase holds when you power down a device of temporarily remove any of the external signals. 

  • A colleague just verified that the quadrature generator inside this part is 2XLO based. This means that it has start up uncertainty. So multiple MAX2771 devices will start up with different phases between the I and Q  LOs. So synchronization is not possible that way. This leaves phase rotation in the digital domain as the only way to achieve phase coherence.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.