Post Go back to editing

hmc8205BF10 Biasing Sequence

Thread Summary

The user is concerned about applying VDD to the HMC8205BF10 power amplifier after measuring a drain-to-source resistance of 10 Ω with a -8 V gate voltage. The final answer suggests carefully turning on the device by setting the power supply to 0V, applying an initial current limit of 650mA, connecting the VDD pins in parallel, setting the gate voltage to -4V, and gradually increasing the supply voltage to 28V while monitoring the current to ensure it does not exceed 500mA.
AI Generated Content
Category: Hardware
Product Number: hmc8205BF10, hmc8205

Hey,

For biasing the HMC8205BF10 power amplifier, I’m following the steps given in the datasheet. When I apply a gate voltage of –8 V, I measure a drain-to-source resistance of about 10 Ω. Should I apply VDD now, or is it risky since the PA costs $800?

  • It's definitely prudent to be careful with turn-on of this device. 

    Are you working with a loose HMC8205BF10 or an evaluation board?  I'm going to suggest that you turn on the chip/board very carefully using the following steps. 

    1. Set the power supply voltage to 0V.

    2. Set an initial current limit on the power supply current at 650mA. 

    3. Connect the (0V) supply voltage to the three VDD pins in parallel.  

    4. Set the gate voltage to -4V.

    5. Start increasing the supply voltage. It should not go above 500 mA (see Fig 50 in datasheet)

    6.  Continue increasing the supply voltage to 28V. It should still be no more than 500mA.

    7. Start increasing VGG, making it more positive, until the target quiescent current is reached.  

  • I have not heard back from you so I'm assuming that you do not need further assistance. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.