Post Go back to editing

The input range for ADL 5904 5910 and ADL 5511

Category: Datasheet/Specs
Product Number: ADL5511

Hi,

We are interested to use ADL5904. ADL 5910 and ADL 5511.

We just want to know the input range for each IC, can you please confirm:

1. ADL5904 : minimum voltage 0V and maximum voltage 5.62V as specified on the datasheet.

2. ADL5910 : minimum voltage 0V and maximum voltage 5.62V as specified on the datasheet.

3. ADL5511:  minimum voltage -2.8V and maximum voltage 2.8v or 5.6V[peak to peak] as specified on the datasheet.

If I follow the range above, I should not damage the IC right? In addition, my frequency input range is from 10 Hz to 10MHz.

Thanks 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.