Post Go back to editing

Write to TX RAM Memory while in RX Mode

Thread Summary

The user inquires about writing to the ADAR1000's RAM transmit beam positions while in RX mode. The final answer confirms that writing to transmit memory locations during RX mode is possible, provided the sequencer is set up correctly and data is written at least 2 beam positions ahead. The engineer also clarifies that writing dummy data to reserved addresses (e.g., 0x1803) is acceptable, and new data can be written to SPI/control registers while the BFIC is transmitting or receiving beam data without interrupting the current operation.
AI Generated Content
Category: Hardware
Product Number: ADAR1000

Hello, 

Fairly new to the ADAR1000. While the ADAR1000 is in RX mode, is it possible to write to the RAM transmit beam positions (RAM starting at 0x1800).
For example, what I am expecting to do it:

- Toggle TR pin to low to activate RX mode

- Write to addresses 0x1800 - 0x180E for the next transmit sequence

- Wait for RX mode time to be over

- Toggle TR pin to high, toggle TX_LOAD as needed

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.