Hello,
I have Question to set 10 dB Attenuator in HMC1122LP4ME parallel mode, in datasheet HMC1122 (Rev. B) page 10 after 8 dB state jump to 16 dB state. I actually need 10 dB attenuator.
Thanks before
HMC1122
Recommended for New Designs
The HMC1122 is a 6-bit digital attenuator operating from 0.1 GHz to 6 GHz with a 31.5 dB attenuation control range in 0.5 dB steps.
The HMC1122 is implemented...
Datasheet
HMC1122 on Analog.com
Hello,
I have Question to set 10 dB Attenuator in HMC1122LP4ME parallel mode, in datasheet HMC1122 (Rev. B) page 10 after 8 dB state jump to 16 dB state. I actually need 10 dB attenuator.
Thanks before
If you want an attenuation of 10 dB, then you just need to engage the 2 dB and the 10 dB attenuator, that is D2 and D4 will be low (active). D0, D1, D3 and D5 will be high (bypassed).