Post Go back to editing

Seeking Interface Solution: Driving HMC8193 IF Port with AD5429 DAC

Category: Hardware
Product Number: HMC8193

Hello, 

I wish to drive the IF port of a HMC8193 (IQ mixer) using a dual channel DAC. I was planning on using a AD5429 to generate IF up to 500KHz (I and Q for the mixer). The data sheet for the quadrature input ports of the mixer in dc coupled applications mentions that these ports should not source or sink more than 6mA. 
Please advise on the interface circuit between the DAC and mixer.


Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.