Post Go back to editing

ADMV85xx Bandpass Filter Output Characteristics

Thread Summary

The user inquires about the ADMV85xx bandpass filters, specifically if they can be considered unamplified switched-capacitor filters, if they modulate or shift the input signal frequency, if they produce output artifacts, and why residual phase noise at a 1 MHz offset from Fcenter is only specified for the ADMV8526. The final answer confirms that the ADMV85xx devices are unamplified switched-capacitor filters, do not modulate or shift the input signal frequency, and can exhibit compression and intermodulation distortion. Residual phase noise plots for ADMV8913 and ADMV8818 are similar to ADMV8526, suggesting comparable performance across the series.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADMV8526

I have some questions about the ADMV85xx bandpass filters.

Can the ADMV85xx devices be thought of as unamplified switched-capacitor filters?

Is the frequency of the input signal modulated or frequency shifted at all by the bandpass filtering process in the ADMV85xx devices?

Does the ADMV85xx filtering process produce any artifacts in the output?

The ADMV8526 datasheets specify the Residual Phase Noise at a 1MHz offset from the center tuning frequency, Fcenter, and show a plot as well. The other similar filters in this ADMV85xx series don't show this information.

Is there some reason these other filters are different? Or do all of the devices meet their typical insertion loss at a 1 MHz offset from Fcenter?

  • To answer your questions:

    Q1. Can the ADMV85xx devices be thought of as unamplified switched-capacitor filters?

    A1. Yes

     

    Q2. Is the frequency of the input signal modulated or frequency shifted at all by the bandpass filtering process in the ADMV85xx devices?

    A2. No

     

    Q3. Does the ADMV85xx filtering process produce any artifacts in the output?

    A3. While the filtering mechanism is passive, the part exhibits compression and intermodulation distortion. 

     

    Q4. The ADMV8526 datasheets specify the Residual Phase Noise at a 1MHz offset from the center tuning frequency, Fcenter, and show a plot as well. The other similar filters in this ADMV85xx series don't show this information.

    Is there some reason these other filters are different? Or do all of the devices meet their typical insertion loss at a 1 MHz offset from Fcenter?

    A4. I'm not sure why some datasheets include it and some do not.  I looked through some other datasheets and did find residual phase noise plots for ADMV8913 and ADMV8818. Both show similar performance to ADMV8526. So I think that you can use these plots as guidance for the family. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.