Post Go back to editing

about AD8304 VNEG current

Thread Summary

The user asked about the driving capability required for VNEG when using the AD8304 with ACOM=0V and VNEG=-0.5V, and an input current of 1mA. The final answer suggests that the VNEG supply must sink the photodiode current, buffer output current, and bias current, totaling up to 15mA for a 10mA photodiode current, given the part's quiescent current of 4.5mA.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD8304

Hi

When using the AD8304 with VNEG and ACOM separated (e.g., ACOM=0V, VNEG=-0.5V, VPS=5V), if the input current to INPT is 1mA, what kind of driving capability is required for VNEG? In other words, what is the maximum current for VNEG?

Thread Notes