Post Go back to editing

about AD8304 VNEG current

Thread Summary

The user asked about the driving capability required for VNEG when using the AD8304 with ACOM=0V and VNEG=-0.5V, and an input current of 1mA. The final answer suggests that the VNEG supply must sink the photodiode current, buffer output current, and bias current, totaling up to 15mA for a 10mA photodiode current, given the part's quiescent current of 4.5mA.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD8304

Hi

When using the AD8304 with VNEG and ACOM separated (e.g., ACOM=0V, VNEG=-0.5V, VPS=5V), if the input current to INPT is 1mA, what kind of driving capability is required for VNEG? In other words, what is the maximum current for VNEG?

Thread Notes

Parents Reply Children
No Data