When AMP1 is set as bypass time, what is the absolute maximum RFIN of the AMP?
ADL6332
Recommended for New Designs
The ADL6332 RxVGA provides an interface from LNA/beam former/
Rx front end to RF analog-to-digital converters (RF-ADC).
Each ADL6332 IC is composed of...
Datasheet
ADL6332 on Analog.com


When AMP1 is set as bypass time, what is the absolute maximum RFIN of the AMP?
GLADION - Moved from Variable Gain Amplifiers (VGA) to RF and Microwave. Post date updated from Wednesday, August 20, 2025 6:33 AM UTC to Wednesday, August 20, 2025 6:48 AM UTC to reflect the move.
GLADION - Moved from Variable Gain Amplifiers (VGA) to RF and Microwave. Post date updated from Wednesday, August 20, 2025 6:48 AM UTC to Wednesday, August 20, 2025 6:48 AM UTC to reflect the move.
Apologies for the delay in responding to you. This question was lost in the system for a few weeks. When you bypass AMP1 the P1dB is “>10 dBm” as you note from the spec table. However there is a foot note that says that this exceeds the absolute maximum rating. This means that the absolute maximum rating for input power comes from somewhere in the input stage and still applies when AMP1 is bypassed.