Post Go back to editing

Out of band performance

Thread Summary

The user inquired about using the ADAR1000 for phase shifting and attenuation at 1 GHz, despite its 8-16 GHz range. The final answer suggests using individual vector modulators or a combination of analog/digital phase shifters and attenuators for 1 GHz signals. For unformed signals, an IQ modulator like the ADL5375 or a complete transceiver like the AD9361 or ADRV9009 is recommended. The accompanying answers note that the ADAR1000's performance degrades significantly at 1 GHz, and synchronization of multiple AD9361 devices requires more than just a common clock, as detailed in a specific thread.
AI Generated Content
Category: Hardware
Product Number: ADAR1000

Hi!

Does anyone know what the out of band performance for the ADAR1000 is? Essentially, this is 8-16GHz part. If you were to attempt to use it lower in frequency, let's say 1GHz, could you still use the attenuators and phase shifters? I understand you would be limited by total phase shift, but could you use this to basically fine-tune a lower frequency phase? Attenuation is probably easier, right? That might be less dependent on frequency?

Thanks!

Parents
  • So for lower frequency arrays, does anyone have a suggestion for individual antenna element attenuation/phase control? It would seem to me the only option would be to use discrete phase shifters and VVAs... But this is not my area of expertise. For very large arrays, is it primarily a game of analog splitting/combining and individual antenna gain/phase control or would a better approach be putting a IQ capable source at each element and do the same with IQ impairments with a shared LO?

Reply
  • So for lower frequency arrays, does anyone have a suggestion for individual antenna element attenuation/phase control? It would seem to me the only option would be to use discrete phase shifters and VVAs... But this is not my area of expertise. For very large arrays, is it primarily a game of analog splitting/combining and individual antenna gain/phase control or would a better approach be putting a IQ capable source at each element and do the same with IQ impairments with a shared LO?

Children
No Data