Post Go back to editing

ADF4360-0: Effect of IC package differences on spectrum spread width during frequency setting

Category: Hardware
Product Number: ADF4360-0


Hello,

Now I post a question that is related for
ez.analog.com/.../adf4360-0-how-to-control-the-hopping-frequency-at-the-settling-to-new-frequency

Now we have requested to the customer which are your suggested three checkpoints.
I'd inform you when we get the results.

There are additional questions from the customer.

1.
As stated in PCN 14_0020 Rev. A, the ADF4360-0 package was changed in 2014.
The package before the change was ‘CP-24-2,’ and the package after the change is ‘CP-24-14.’
When customers measured the frequency spectrum, including the transient response during VCO calibration, by setting the spectrum analyser to peak hold mode and performing a step sweep in the 2.4 GHz to 2.5 GHz range, they found that the ‘CP-24-2’ and ‘CP-24-14’ packages exhibited significantly different characteristics.

CP-24-14 package (after PCN 14_0020 Rev. A)


CP-24-2 package (before PCN 14_0020 Rev. A)


The customer wants to know whether the difference in the spread of the frequency spectrum is due to individual differences in the ADF4360-0, or whether it is a difference between the ADF4360-0 before PCN and the ADF4360-0 after PCN.
If this difference is due to individual differences in the ADF4360-0, this customer says that they cannot use the ADF4360-0.

Even with ADF4360-0 after PCN, is it possible for the spectrum to spread out like ‘ADF4360-0_2.png’?


2. Changing the VCO current value of the ADF4360-0 changes the spectrum spread width when performing a step sweep. Does this spread width show the same trend even when replacing the unit?
In the ADF4360-0 after PCN, the spread of frequency spectrum differs between settings of 15 mA and 20 mA for the VCO current.

VCO current: 15mA.


"VCO current: 20mA


When he set the VCO current to 20 mA, the frequency spectrum spread looks like narrower than when it was 15 mA.
When using step sweeping, the customer wants to narrow the frequency spectrum spread, but will the relationship between the VCO current and the frequency spectrum spread remain the same even if the device is changed to other ADF4360-0??
(Has it been confirmed in the design data that increasing the VCO current tends to prevent the spectrum from widening?)

Settings of ADF4360-0 are as follows:
- Reference: 10MHz
- R counter: 100
- PFD freq.: 100kHz
- Frequency step for sweep:100kHz
- Start frequency: 2.4GHz
- Stop frequency: 2.5GHz
- Loop filter BW: 6.25kHz

Loop Filter:


Output circuit:


If you need more information to consider this behavior, please let me know.
Best regards,

y_suzuki

Edit Notes

I added the pictures.
[edited by: y_suzuki at 1:34 PM (GMT -4) on 24 Jul 2025]
  • Hi Suzuki,

    Does this problem only occur in sweeping mode? Do both devices work properly when set to frequencies manually?
    I checked the loop filter and design parameters, and they look okay.

    This PCN refers to package changes, performance variation is not expected.  My first opinion is it is about band selection, similar to the previous issue. Let me check if any Autocal parameter has changed during this change.

    Regards,
    Burhan

  • Hello Burhan,

    I appreciate your support.

    > Does this problem only occur in sweeping mode? Do both devices work properly when set to frequencies manually?

    I wrote ‘sweep,’ but in reality, the frequency is increased by 100 kHz at a time.
    Each frequency is set, and after autocal is completed, the output is at the correct frequency.

    > This PCN refers to package changes, performance variation is not expected.

    If the IC package is changed and the lead frame is changed, I think the bonding wire will also change. Could this difference be having an impact?

    The register settings are the same for all devices.
        R counter Latch: 0x300191
        Control Latch: 0x4FF12C
        N counter Latch: (example)
            2400MHz: 0x05DC02
            2401MHz: 0x05DC2A
            2450MHz: 0x05FB12
            2500MHz: 0x061A22

    BCS[1:0]=11b, the band select clock divider is 8.
    Is there any other information you need?

    Best regards,

    y_suzuki

  • Hello Burhan,

    I have two questions this time.
    Regarding ‘1.’, is the conclusion that it is unlikely that the frequency hopping width during autocal will change due to the package change?

    Regarding the second question above, the customer is interested in the relationship between VCO current and the frequency hopping width during autocalibration.  
    The customer compared cases where the VCO current was set to 15mA and 20mA, and confirmed that the hopping width was smaller at 20mA.
    Is there a possibility that this trend could reverse if the device is replaced?

    Best regards,

    y_suzuki

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.