In the LT5538 datasheet the electrical specifications are given only for 5V supply voltage. The chip is specified to work from 3V to 5.5V. I want to use 3.3V voltage supply. Are the characteristic curves the same?
LT5538
Production
The LT5538 is a 40MHz to 3800MHz monolithic logarithmic RF power detector, capable of measuring RF signals over a wide dynamic range, from –75dBm to...
Datasheet
LT5538 on Analog.com
In the LT5538 datasheet the electrical specifications are given only for 5V supply voltage. The chip is specified to work from 3V to 5.5V. I want to use 3.3V voltage supply. Are the characteristic curves the same?
There are three plots in the datasheet that compare operation at 3V and 5V. You will get very similar performance at 3.3V. The temperature stability at 3.3V is going to be very similar to the performance at 5V that is shown in the datasheeet.
Eamon
There are three plots in the datasheet that compare operation at 3V and 5V. You will get very similar performance at 3.3V. The temperature stability at 3.3V is going to be very similar to the performance at 5V that is shown in the datasheeet.
Eamon