I've recently bought an ADL5961 evaluation board for testing, but I'm getting unanticipated IF outputs. The differential incident peaks out at about 32mVpp, regardless of IGAIN, and the reflected is much lower than expected - some 7dB or more lower. It responds better to the RGAIN setting, but seems to max out at 32mVpp differential into two 50R oscilloscope inputs - when I believe the datasheet says they should max out at 8Vpp differential.
My test setup is as follows:
HARDWARE:
HP54542A oscilloscope - using all four inputs, each set to 50R, and using a MATH function to create the differential voltages. Ch 1 and 2 are connected to IFFP and IFFM respectively, Ch 3 and 4 connected to IFRP and IFRM respectively. My math functions do Ch1-Ch2 and Ch3-Ch4.
My RF source is a Marconi 6311, which is outputting a 3dBm signal at 10GHz in CW mode. This goes into a Midwest Microwave divider (PWD-5530-02-SMA-79) which is rated for up to 10W between 0.5 - 18 GHz. From one output, the signal is routed through a minicircuits DC block (BLK-18-S+) into the RFIN port of the Eval circuit, J1. The RFOUT also has the same minicircuits DC block on the output.
The second output from the power divider is routed directly into LOP. LOM is terminated in a 50R termination.
I wish to run the ADL5961 in offset mode. To do this I have attached the output from a Agilent 33120A sig gen directly to the OFP input, driven at 10MHz at 100mVpp. OFM is left open - I see on the eval schematic it is tied to GND via 50R resistors - so the differential input voltage should be 200mVpp - which is comfortably within the datasheet specs.
Power is provided by 5V supply - during use the device draws around 160mA of current.
The ADL5961 eval is connected to the Linduino through the ribbon cable, and power up/down sequence followed as per the guide here: https://wiki.analog.com/_media/resources/eval/user-guides/ug-adl5960_20220415_draft.pdf
SOFTWARE:
In the eval software, BYPASS mode is 0 (OFF), LOMODE is 1 (x1), OFMODE is 0 (x1 - no dividers enabled).
RESULTS:
The differential waveforms appear as square waves - the incident reaches 32mVpp differential easily - the reflected needs 18dB of gain to achieve the same. I would expected the reflected differential to be slightly lower to account for insertion loss, but this is only about 2dB by the datasheet. As an example, with both IGAIN and RGAIN at 0, the incident differential voltage is 30mVpp, the reflected is 7.5mVpp.
The output frequency is correct at 10MHz.
Compare incident and reflected differential IFs, I get the expected 180-degree phase-shift when comparing short and open on the test port. However, connecting a 50R load doesn't really attenuate the reflected wave by much.
QUESTION:
What should I expect to see given these inputs? Have I incorrectly configured the device/inputs? I am most puzzled by the large discrepancy between the incident and reflected differential IF levels, as well as not noticing a substantial difference between OPEN and LOAD tests.
I would be very happy to provide measurement data, photos and as much additional data as required to help.