Post Go back to editing

HACKRF

Thread Summary

The user is experiencing lower than expected output power (24.5 dBm) with the HMC409LP4E at 3.6 GHz and 4 dBm input power. The final answer suggests checking the power supply, ensuring it can source up to 1 Amp, and verifying the correct VCC and VBIAS voltages. A power sweep test is recommended to diagnose the issue further.
AI Generated Content
Category: Hardware
Product Number: HMC409LP4E, HMC409

Hi ADI engineer

I use the HMC409LP4E for RF_TX, the frequency is 3.6GHz, the power of RFIN is 4dBm,but the power of RFOUT only 24.5dBm.

I try to reduce the RFIN power to -10dBm, Gain can up to 29dB.

I find the Gain is 31dB,P1dB is 30.5dBm RFIN_MAX is 10dBm in datasheet. So i think the RFOUT can up to 30.5dBm

But RFOUT only 24.5dBm,the gain only 21.5dB(24.5-4) when RFIN at 4dBm.

Is there some wrong in my design? or I misunderstood?

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.