Post Go back to editing

Relative phase data of HMC1119

Thread Summary

The user requested relative phase variation data for the HMC1119 at 3.5 GHz. The support engineer provided an S-parameter file with the correct data, clarifying that the file name initially contained an internal part number but has been corrected to include HMC1119. The data includes phase variation (S21ang) in degrees and covers frequencies from 10 MHz to 6 GHz at 3.3V and 5V supply voltages for 10 devices.
AI Generated Content
Category: Hardware
Product Number: HMC1119

Hi,

Can you provide relative phase variation data for the HMC1119 around 3GHz to 3.5GHz (3.5GHz is better)?

Best regards,

Akira