Post Go back to editing

Can the LTC5553 support RF frequencies as low as 500 MHz?

Category: Hardware

Hi Team,

I’m using the LTC5553 to down-convert RF signals to a 1.5 GHz IF, but the RF input spans from 500 MHz to 10 GHz. The datasheet specifies that the RF port is well-matched only from 3 to 20 GHz. Can you clarify what happens between 500 and 3000 MHz?

Thankyou

Thread Notes