Hello,
I lack previous experience with PFD/PLL designs, but my understanding is that the PFD should not respond in any significant way to the signal amplitudes, assuming that they are within the input range.
I have a custom design with HMC439. For testing purposes, I have disconnected NU & ND from the lowpass circuit, leaving only the pullup resistors, so I can observe the digital output on scope. REF is currently driven from a dual-channel AWG via an ADT1-1 transformer with one side of the secondary grounded , both then decoupled via 1nF capacitors and routed as a 50Ohm differential pair to the REF/NREF pins. I set the power in -10dBm .. 10dBm range as specified. The VCO is driven from another AWG channel through a resistive power splitter, with once again the NVCO grounded via a capacitor. The power is in ~ -6dBm..-10dBm range. I set the frequencies on the AWG a tiny bit apart, so I can observe the output over phase difference. The rest of the circuit is configured as in datasheet example, with VCC3V driven via a 200Ohm resistor from 5V (is there a reason there is no decoupling capacitor on this pin btw?). The frequency range I'm using is 10..40MHz.
The thing is: for most of the amplitude ranges of REF, I observe exclusively pulses on NU or ND but never at both over all phase relationships. If I fiddle with REF amplitude, it flips between only-NU or only-ND but never both. Reducing the amplitude on VCO will allow for both to work, but it should be well within the allowed range of -10dBm .. 10dBm already. Interestingly, with RF completely removed, one of the pins seems to be sinking some constant current, but not quite that of a usual pulse..
I've also tried replacing the IC in case there was an ESD issues, with same behaviour.
Am I misunderstanding the function and this is a sensible output or what could be the cause in circuit?