Dear ADI EngineerZone
I want to include the HMC311SC70ETR (gain block RF amplifier) within a LTSPICE simulation. However, I am unable to find a SPICE model (nor indeed a schematic).
Please advise on how I can do this.
Thank you + best wishes
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
HMC311SC70
Last Time Buy
The HMC311SC70(E) is a GaAs InGaP Heterojunction Bipolar Transistor (HBT) Gain Block MMIC SMT DC to 8 GHz amplifier. Packaged in an industry standard SC70...
Datasheet
HMC311SC70 on Analog.com
Dear ADI EngineerZone
I want to include the HMC311SC70ETR (gain block RF amplifier) within a LTSPICE simulation. However, I am unable to find a SPICE model (nor indeed a schematic).
Please advise on how I can do this.
Thank you + best wishes
Hi Hugh, I checked with my colleagues in the LTSpice group and they confirmed that you cannot simulate an RF amplifier in LTSpice. LTSpice is an analog domain simulator that is at home with voltage and time domain simulations of devices such as operational amplifiers which have high input impedance and low output impedance. HMC311 is an RF amplifier with with input and output impedance of 50 ohms and behavior that is best modelled in the logarithmic power domain (e.g. output power in dBm, gain and noise in dB). So there are no structures in place in LTSpice to support rf components such as an RF Amplifier.
I think that if you wanted to, you could build a basic model from scratch. You would start with a block of gain. At the input you would add a 50 ohm resistor to ground. And at the output, you would add a 50 ohm series resistor to give the device and output resistance of 50 ohms. If you need to model HMC311 in your system to complete the signal chain, something like this might work.
Best Regards
Eamon Nash
Hi again Hugh,
I need to correct myself. It seems that there is a process to pull s-parameter datasets into LTSpice. See the thread below which links to an external groups.io group where a process is described. I have not tried this but I would like to at some point becuase the question comes up from time to time.
Best Regards
Eamon