Post Go back to editing

Output impedance of the Vlog Pin of AD8309

Thread Summary

The user inquired about the output impedance of the VLog pin on the AD8309 IC for interfacing with an ADC. The support engineer clarified that the output resistance is 0.3 Ohms, and suggested using a differential amplifier like the ADA4945-1 to convert the single-ended output to a differential signal, scale the voltage, and set the common mode voltage. No impedance matching is necessary due to the low output resistance of the AD8309.

View FAQ
AI Generated Content
Category: Hardware
Product Number: AD8309

Hi,

We wanted to interface the AD8309 IC's VLog pin to an ADC. For this we require the output impedance of the Vlog pin of AD8309 for the driver and other interface. However, only the output resistance (0.3 Ohms) is mentioned in the datasheet. We are unable to infer the output impedance of the Vlog pin from the datasheet. Could anyone please help on this ?

Regards,

ARK

  • Hello, 

    Could anyone please suggest something on this ?

    Regards,

    Avinash

  • Hi Avinash,

    I'm guessing that you want to know the complex impedance of the VLOG output, that is, where is it on the Smith Chart. This is not really the correct way to think of this output. The output is more like an op-amp output (i.e. ideally 0 Ohms output resistance) than an RF Amplifier output (i.e. close to 50 ohms with some capacitance or inductance). So you should not be trying to do any kind of an impedance match between the AD8309 and the ADC. Since the AD8309 has such low output resistance, it should be possible to connect it directly to the ADC input if the ADC's input resistance is relatively high, say greater than 500 ohms. Alternatively, you could put an op-amp buffer between the two devices, particularily if the ADC input is a switching capacitive load. 

    Best Regards

    Eamon

  • Thanks a lot Eamon, for correcting my understanding,

    So we can just convert the signal output of the Vlog from the AD8309 to the ADC input range via a driver and connect it to the ADC. Since our ADC expects a differential input, we will need to connect a differential amplifier in between. Hence we wanted some understanding on the impedance.

    From your above answer, we shall reduce the signal range of the AD8309 to match the ADC input and use a differential buffer in between.

    Thanks for the answer.

  • Hi Avinash,

    yes, that all makes sense. Your diff amp needs to do three things. It needs perform a single-ended to differential conversion. It needs to scale the AD8309 output voltage appropriately so that it maps to the input range of the ADC. And it need to set the common mode voltage of the differential signal so that it maps to the expected common mode input level of the ADC. ADA4945-1 looks to me like a good choice. (https://www.analog.com/en/products/ada4945-1.html). 

    There are lots of other good options to consider also. Take a look at this selection table (Single-Ended to Differential Amplifiers | Analog Devices).

    There is a calculator tool available for dimensioning the diff amp design (ADI-DiffAmpCalc | Analog Devices).

    Best Regards

    Eamon

     

    hanks a lot Eamon, for correcting my understanding,

    So we can just convert the signal output of the Vlog from the AD8309 to the ADC input range via a driver and connect it to the ADC. Since our ADC expects a differential input, we will need to connect a differential amplifier in between. Hence we wanted some understanding on the impedance.

     

    From your above answer, we shall reduce the signal range of the AD8309 to match the ADC input and use a differential buffer in between.

     

    Thanks for the answer.

  • Thanks a lot EaMon.

    We intend to use ADA4938-1 for our ADC LTC2256-14.

    The ADC can have an input range of 2V(p-p) & a common mode voltage of 0.9V (1.8V is the VDD). Hence the swing at the ADC input can be 0.4 to 1.4V (Vcm - 0.5V to Vcm + 0.5V).

    The Vlog output of the Log Amplifier can swing typically between 0.4V to 2.4V. So, we intend to provide a gain of 0.5 for the differential amplifier so that the output from the Log detector can be scaled to 0.2V to 1.2V at the ADC input. We intend to achieve this through a (feedback resistor/ input Resistor) ratio of 0.5. Hence the chain is as follows:

    Log Detector ---> Differential Amplifier(ADA4938-1) ---> ADC (LTC2256-14)

    Is the above understanding correct. Or should there be a buffer amplifier in between the Log Detector and the differential amplifier?

  • Hi Avinash,

    that sounds like a good plan. I don't think that you need a buffer amplifier between the AD8309 and the diff-amp. Just be cognizant of the current demand on AD8309. Your configuration may call for the AD8309 to sink current. The datasheet says that the part can sink 1mA and source around 50mA. So you may need to adjust the resistor sizes around the diffamp accordingly. Also I would check in the diff amp calculator or in LTSpice that the diff amp can indeed handle a closed loop gain of 0.5. It might be good to hit the diff amp with step response in LTSpice to ensure that it doesn't have excessive ringing. 

    Best Regards

    Eamon

  • Hi Eamon,

    Thanks for the answer. We checked in the diff amp calc with the gain of the ADA4938 at 0.5, however, it suggested that the gain cannot be too less due to instability of the amplifier. We checked with LT-SPICE, but it wouldn't show anything on the stability.

    Instead, to be on a safer side, we are thinking of using a voltage divider at the output of the AD8309 for equal division, to get the voltage range of the AD8309 to that of the ADC and then use the differential amplifier with a gain of 1. We can also use a buffer in between the voltage divider and the amplifier for stability.

    Hence the chain will look as follows:

    AD8309 (0.4V to 2.4V) --> Voltage Divider (0.2V to 1.2V) --> Non Inverting Amplifier (Gain = 1) -->Differential Amplifier(ADA4938-1) (Gain of 1) ---> ADC (LTC2256-14)

    However, I do not know the implications of using this, especially wrt the stability/noise due to the use of the voltage divider. 

    When we checked with the Differential amp that you had suggested (ADA4945-1), we were able to get the gain even below 0.5 to be stable in Diff Calc, but trying in the LT-SPICE ended nowhere as it requires various signals such as clamp and disable. We tried using signal ranges provided in the datasheet, but it didn't give us appropriate results due to which we are apprehensive to use the device for further analysis, owing to time shortage.

    Request you to please provide your inputs on the chain.

    Regards,

    ARK

  • Hi Avinash,

    the (Log-Amp→Voltage Divider→G+1 Buffer→G+1Diff Amp) is conservative and completely un-problematic. Just select an op-amp that is unity gain stable that operates from a single supply (e.g. ADA4805-1). 

    Eamon

     

     

     

     

    Hi Eamon,

    Thanks for the answer. We checked in the diff amp calc with the gain of the ADA4938 at 0.5, however, it suggested that the gain cannot be too less due to instability of the amplifier. We checked with LT-SPICE, but it wouldn't show anything on the stability.

    Instead, to be on a safer side, we are thinking of using a voltage divider at the output of the AD8309 for equal division, to get the voltage range of the AD8309 to that of the ADC and then use the differential amplifier with a gain of 1. We can also use a buffer in between the voltage divider and the amplifier for stability.

    Hence the chain will look as follows:

    AD8309 (0.4V to 2.4V) --> Voltage Divider (0.2V to 1.2V) --> Non Inverting Amplifier (Gain = 1) -->Differential Amplifier(ADA4938-1) (Gain of 1) ---> ADC (LTC2256-14)

    However, I do not know the implications of using this, especially wrt the stability/noise due to the use of the voltage divider. 

    When we checked with the Differential amp that you had suggested (ADA4945-1), we were able to get the gain even below 0.5 to be stable in Diff Calc, but trying in the LT-SPICE ended nowhere as it requires various signals such as clamp and disable. We tried using signal ranges provided in the datasheet, but it didn't give us appropriate results due to which we are apprehensive to use the device for further analysis, owing to time shortage.

    Request you to please provide your inputs on the chain.

    Regards,

    ARK

  • Thanks a lot Eamon, we shall consider this in our simulation in LTSPICE and the DiffAmp tool as well. We are trying to arrange for some samples of the differential amplifier and we want to try this setup in our lab as well. I shall post further updates.

    Regards,

    Avinash

  • Hi EaMon,

    We have done a simulation using LT-SPICE of the entire device chain using ADA4805 OP-AMP as buffer and ADA4938 as the Differential Amplifier.

    The simulated output for a pulse of 2.4V with a rise-time of 20nsec and a pulse width of 300nsec, is as follows & it is within the input range of the ADC: 

    However, there seems to be an issue with the rise and the fall times of the pulses, as they are tending to overshoot. This could be a problem at our measurements, as we anticipate a single pulse at the output. Is there any way that this could be reduced practically? 

    Regards,

    Avinash

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.