Post Go back to editing

ADTR 1107 Datasheet concern

Thread Summary

The user is concerned about using a power supply with a minimum current output of 1 mA for the ADTR1107 control supply pins (IDD_SW and ISS_SW), which typically draw microamp currents. The final answer clarifies that the power supply's current limit should be set to a safe level above the device's operating current (e.g., 25 μA for VDD_SW and 150 μA for VSS_SW) to protect against overvoltage, and that the actual current drawn will be determined by the device's input impedance. The user's power supply can be used without external circuitry, provided the voltage is set to the specified value (+/-3.3V) and the current limits are appropriately configured.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADTR 1107

I was testing the ADTR1107 on the transmit side, and I observed that the datasheet specifies the control supply currents—such as IDD_SW and ISS_SW—to be in the microamp range. However, the datasheet does not state the absolute maximum current ratings for these supply pins. My concern is that the power supply I am using has a minimum current output capability of 1 mA, which is significantly higher than the typical current these pins draw. I would appreciate clarification on whether it is safe to use such a power supply and whether external load resistors or current sinks are required to ensure proper voltage regulation and stable operation.

Additionally, in the event that the device is not functioning correctly despite aiming for microamp-level currents, is it permissible to supply a slightly higher current—such as in the milliamp range—for testing purposes? If so, how much current (in milliamps) is considered safe for these control supply pins without risking damage to the device?

Thank you for your support and guidance.

Thread Notes

  • Hi Izaan,

    I will check into your question and will get back to you as soon as possible.

    Best Regards

    Eamon

  • Hi Izaan,

    You don't need to worry about applying a maximum current. That is not how these devices work. When you apply the recommended supply voltage to the ADTR1107 switches, a certain current will flow based on the effective input impedance of the VDD_SW and VSS_SW pins. As long as you keep the voltage on these pins below their abs max ratings (+3.6V and -3.6V), the normal currents (14uA and 120uA respectively) will flow. If you take the voltages beyond +3.6 V and -3.6V, then excessive currents may start to flow and the part will probably get damaged. 

    On your power supply, you generally have the ability to limit the amount of current that can flow. So in your case, you could set the positive limit to, say 25uA and the negative limit to, say 150uA. That doesn't mean that these current levels will actually flow. It just means that if you accidentally turn the postive supply voltage up to 5V, the increasing current will clamp at 25uA which will probably save the device. 

    Best Regards

    Eamon

  • Hi Eamon,
    Thank you for your response. I have a question—my DC power supply has a minimum current limit of 1 mA, so I’m unable to supply 25 microamps directly. I would prefer not to use any external circuitry to reduce the current. Given this, what options do I have?
    Best Regards
    Izaan

  • Hi Izaan, you are missing my point and focusing incorrectly on the current capabilities of your power supply. The only funciton of the current display on your voltage mode power supply (I assume that you are using a voltage mode power supply) is to set a current limit in case something goes wrong. So set the volage to the specified value (+/-3.3V) and set the max current at some level that is higher than the specified operating current for the device.

    Eamon

  • Hi Eamon,
    Thank you for your response. I got it, but Im also facing a strange behavior as the max current VDD_SW can draw according to datasheet is 14µA but in my case it is drawing currents in milliamps approx 10 to 20 mlliamps well is that suitable for the chip? and if im getting to much current form the switch what could i do?
    Best Regards
    Izaan