- In ADRF5730 , What will be it's Default RF Attenuation if PS pin is Pulled High and LE pin is Pulled High, After Turing on VDD and VSS ?
ADRF5730
Recommended for New Designs
The ADRF5730 is a silicon, 6-bit digital attenuator with 31.5 dB attenuation control range in 0.5 dB steps.
This device operates from 100 MHz to 40 GHz...
Datasheet
ADRF5730 on Analog.com
Hi Surya, I just verified with a colleague that the ADRF5730 part will remain in max attenuation when LE and PS are pulled high after the part is powered-on.
Eamon