Post Go back to editing

Phase changing

Category: Hardware
Product Number: ADL5387

Good afternoon,

I would like to share with you a problem that we have in an equipment that we are developing. This equipment has a receiver for an RF input. We are using three of your devices in the receiver stage, the HMC686LP4 mixer, the AD8309 demodulating logarithmic and the ADL5387 demodulator. You can see the schematic in the following figures.

The problem we are having, is that the signals coming out from the ADL5387 (QHI, IHI) change its phase 180º randomly, while we are transmitting. We have the input of the receiver connected to an I/O device that reflexes part of the transmitted power, and we have detected that the phase only changes when we are transmitting. We suspect that this reflected power is the founder of this problem, but we have a proper filtering to the bandwidth of transmission frequency.

We would be very thankful to you if you can provide us some clues on why this device, ADL5387, change the phase of its outputs. As well, under which conditions or setup this device phase changing needs to happen.

Thank you very much!

Parents
  • Hi Adrian,

    we don't have a similar IC that is pin-compatible with ADL5387. If you think that you are losing phase because external interference, there are a few additional experiments that you could try. 

    1. Try to turn off the other components in the signal chain.
    2. Try some rudimentary shielding to see if this has an impact. 
    3. Apply a high powered external LO. Take the power level close to the abs max ratings spec, just for testing purposes. If you find that the problem goes away if the LO power is very strong, that would tend to suggest that the problem is indeed leakage and/or interference. 

      Best Regards

      Eamon Nash

Reply
  • Hi Adrian,

    we don't have a similar IC that is pin-compatible with ADL5387. If you think that you are losing phase because external interference, there are a few additional experiments that you could try. 

    1. Try to turn off the other components in the signal chain.
    2. Try some rudimentary shielding to see if this has an impact. 
    3. Apply a high powered external LO. Take the power level close to the abs max ratings spec, just for testing purposes. If you find that the problem goes away if the LO power is very strong, that would tend to suggest that the problem is indeed leakage and/or interference. 

      Best Regards

      Eamon Nash

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.