Post Go back to editing

max2706

Thread Summary

The user is experiencing a significant drop in the regulator's output voltage when connecting both the VTUNE and VCC pins of a VCO circuit. The final answer suggests testing with a low impedance voltage source directly on the VTUNE pin to diagnose the issue. The accompanying answer recommends checking for excessive current draw by applying voltages from external power supplies to the VCC and VTUNE pins separately, with current limits set, to identify potential damage or excessive current consumption.
AI Generated Content
Category: Hardware
Product Number: MAX2607

Hello!

I've designed a VCO circuit on a general-purpose board. As I mentioned earlier, due to certain limitations, I can't use a PLL circuit to supply the VTUNE voltage. Instead, I'm supplying VTUNE through a voltage divider.

However, when I connect the 2.7V output of the regulator to both the VTUNE pin and the VCC pin, the regulator's output voltage drops significantly. But if I disconnect either the VTUNE or the VCC pin, the regulator output returns to 2.7V.

What could be the issue? Can you please provide some helpful suggestions that might actually work?

Parents
  • Hi Harshkumar,

    regarding your question about using a voltage divider to generate the Vtune voltage, the current into the Vtune pin is very low. So I don't see a problem with your approach. As a test, you could try feeding a low impedance voltage (e.g. from a power supply) directly on to the Vtune pin to see if this makes a difference. I don't expect that it will but worth an experiment. - Eamon

Reply
  • Hi Harshkumar,

    regarding your question about using a voltage divider to generate the Vtune voltage, the current into the Vtune pin is very low. So I don't see a problem with your approach. As a test, you could try feeding a low impedance voltage (e.g. from a power supply) directly on to the Vtune pin to see if this makes a difference. I don't expect that it will but worth an experiment. - Eamon

Children
  • Hi Enash,

    I need your guidance on a few critical points regarding the MAX2607 VCO setup.

    Will the VCO circuit function properly if assembled on a general-purpose board or zero PCB? Can I still expect an output in the 100 MHz to 300 MHz range, which is the specified range for the VCO?

    Also, do I need to use a spectrum analyzer for accurate measurement, or will a DSO with bandwidth greater than 300 MHz suffice? I'm also concerned about the impedance of the probe — could that be affecting the output? Right now, I’m only seeing a 50 Hz signal, which is far off from the expected range.

    Even if there’s a mismatch in the inductor or capacitor values, shouldn’t the output still fall somewhere within the VCO’s operating frequency range? Please advise on this.

    Today, I’m planning to assemble the complete circuit on the actual designed PCB (15 mm size). and observe the current Given that the deadline has already passed, I kindly request a final working solution from your side.

    and

    If there’s an alternative to the VCO that can generate the required frequency and transmit at around -10 dBi, please suggest it.

    If possible, I would really appreciate a quick live call or chat to resolve this efficiently.

    Looking forward to your urgent support.

    Best regards,

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.