Post Go back to editing

max2706

Thread Summary

The user is experiencing a significant drop in the regulator's output voltage when connecting both the VTUNE and VCC pins of a VCO circuit. The final answer suggests testing with a low impedance voltage source directly on the VTUNE pin to diagnose the issue. The accompanying answer recommends checking for excessive current draw by applying voltages from external power supplies to the VCC and VTUNE pins separately, with current limits set, to identify potential damage or excessive current consumption.
AI Generated Content
Category: Hardware
Product Number: MAX2607

Hello!

I've designed a VCO circuit on a general-purpose board. As I mentioned earlier, due to certain limitations, I can't use a PLL circuit to supply the VTUNE voltage. Instead, I'm supplying VTUNE through a voltage divider.

However, when I connect the 2.7V output of the regulator to both the VTUNE pin and the VCC pin, the regulator's output voltage drops significantly. But if I disconnect either the VTUNE or the VCC pin, the regulator output returns to 2.7V.

What could be the issue? Can you please provide some helpful suggestions that might actually work?

Parents Reply Children
  • Hey Enash,

    First of all, the voltage regulator I’m using has a maximum current supply capacity of 150 mA, so I don’t think that should be an issue.

    I just want to clarify one thing— is the circuit I shared okay or not?
    Also, I’m currently supplying the VTUNE pin using a voltage divider. Will that work or not?

    Please just let me know about this for now. Meanwhile, I’ll work on your previous suggestion to use an external dual power supply.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.