Post Go back to editing

max2706

Thread Summary

The user is experiencing a significant drop in the regulator's output voltage when connecting both the VTUNE and VCC pins of a VCO circuit. The final answer suggests testing with a low impedance voltage source directly on the VTUNE pin to diagnose the issue. The accompanying answer recommends checking for excessive current draw by applying voltages from external power supplies to the VCC and VTUNE pins separately, with current limits set, to identify potential damage or excessive current consumption.
AI Generated Content
Category: Hardware
Product Number: MAX2607

Hello!

I've designed a VCO circuit on a general-purpose board. As I mentioned earlier, due to certain limitations, I can't use a PLL circuit to supply the VTUNE voltage. Instead, I'm supplying VTUNE through a voltage divider.

However, when I connect the 2.7V output of the regulator to both the VTUNE pin and the VCC pin, the regulator's output voltage drops significantly. But if I disconnect either the VTUNE or the VCC pin, the regulator output returns to 2.7V.

What could be the issue? Can you please provide some helpful suggestions that might actually work?

Parents
  • Hi Harshkumar,

    at first glance, I do not see that you are doing anything wrong. Did the component values that you are using come from the evaluation board schematic? It seems that the VCO is lots of  current, more current than the LDO can deliver. Here are some experiments you could try. 

    1. Apply a voltage from an external power supplpy to the VCC pin (leave VTUNE open). Set a current limit on the power supply of around 10mA. If this current limit triggers, there is a possibility that your part is damaged.
    2. If you do not get excessive current, apply a second voltage to the Tune Pin and set the limit on this current to, say, 1mA.  Turn on your two voltages and see what current is flowing from each source. If you are using two separate power supplies, connect the grounds together.
    3. During this testing, connect the output to a spectrum analyzer to see if you are getting any outupt signal. 

    Please try these experiments and let me know if you make any progress. 

    Best Regards

    Eamon Nash

Reply
  • Hi Harshkumar,

    at first glance, I do not see that you are doing anything wrong. Did the component values that you are using come from the evaluation board schematic? It seems that the VCO is lots of  current, more current than the LDO can deliver. Here are some experiments you could try. 

    1. Apply a voltage from an external power supplpy to the VCC pin (leave VTUNE open). Set a current limit on the power supply of around 10mA. If this current limit triggers, there is a possibility that your part is damaged.
    2. If you do not get excessive current, apply a second voltage to the Tune Pin and set the limit on this current to, say, 1mA.  Turn on your two voltages and see what current is flowing from each source. If you are using two separate power supplies, connect the grounds together.
    3. During this testing, connect the output to a spectrum analyzer to see if you are getting any outupt signal. 

    Please try these experiments and let me know if you make any progress. 

    Best Regards

    Eamon Nash

Children
  • Hi Eamon,

    I followed the steps you provided and measured the currents successfully:

    • VCC is drawing between 2.3 mA to 2.65 mA

    • VTUNE is drawing around 0.09 mA to 0.10 mA

    So far, everything seems within expected limits.

    Now, I need your guidance on how to properly check the output signal.

    1. What exactly should I connect at the OUT+ and OUT- pins to observe the VCO output?

    2. I'm not planning to use the VCO in a differential (bi-directional) configuration, so could you please advise the correct setup for single-ended output measurement?

    3. Should I connect OUT+ through a coupling capacitor directly to a spectrum analyzer or high-bandwidth oscilloscope?

    4. Do I need to leave OUT– floating, grounded, or terminated in some way when not using it?

    Your suggestions on the correct configuration would really help me move forward.

    Thanks in advance for your support!

    Best regards

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.