Post Go back to editing

hmc833 can not locked

Category: Software
Product Number: HMC833

Hello,

The chip of hmc833 can not locked. The ref_clock is 100MHz. The ouput clock is around 5GHz, but not stable. It is shifting left and right. 

The registers are set as below:

x"00000020" &
x"0F000081" &
x"02000001" & -- reference divider 2,1
x"062003CA" & -- bit7=1 to bypass;bit11=0 to disable frac part
x"095FF972" &
x"0A002046" &
x"0B07C021" &
x"0500e090" & -- (vco reg 2) 1 11 000001 0010 000
x"05001628" & -- (vco reg 5) 0 00 10 11 00 0101 000
-- x"05002898" & -- (vco reg 3) 00?0 10 0 0 0 1 0011 000 fundamendal mode
x"05002018" & -- (vco reg 3) 00010 00 0 0 0 0011 000 doubler mode
x"050060A0" & -- (vco reg 4) 01 10 00 001 0100 000
x"05000000" & -- (vco reg 0) - leave at 0
x"03000019" & -- int Reg; 0x32 = 50,25
x"04000000"; -- frac part

Could you please show me how to fix this problem? Thank you very much for your support in advance!

Best regards,

Howard

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.