Post Go back to editing

Accuracy / Tolerance / dBm to mV

Category: Datasheet/Specs
Product Number: LT5538

Hi Support

I have inherited a power detector circuit that uses the LT5538 power detector.

Across multiple DuTs I measure the response of the detector in 2dB steps from -5dBm down to -15dBm, or so, in order to derive the 'linear' gradient (m) and intercept (c) response: as y=mx+c [with y in mV, m in mV/dB, x in dBm and c in mV].

There are two plots that seem relevant:

1) Slope Distribution vs Temperature at 2.14GHz == distribution of mV/dB (ie. m)

2) Logarithmic Intercept Distribution vs Temperature at 2.14GHz == distribution of extraplolated intercept 0mV point

As the gradient and intercept points are correlated it is hard to gauge how the intercept point relates to a linear response whose c term is determined at 0dBm. There >12dB spread in the extrapolate data for 0mV. Is this also seen in the 0dBm c term? 

The Vout v IP Power Plots suggest the power detector does not suffer from a wide spread in the c term. The reason I ask is that I am trying to establish production limits for the c term at 2.5GHz and also want tor determine if I have ESD components (such as RF switches or even the power detector itself).

Are you able to enlighten me as the 6 sigma spread I might expect for the c term please? And also what the ESD rating is for the LT5538?

Many thanks

Parents
  • Hey  ,

    Your understanding is correct, that spread you are seeing in the intercept will be seen at 0dBm as well. Below, I've clipped the response of the ADL5506 which has some more detail, but you can see the relationship between the intercept/slope and the response at higher power.


    I don't have the spread for the intercept point for this part, and the ESD rating is 1.5kV HBM and 1kV CDM. 

Reply
  • Hey  ,

    Your understanding is correct, that spread you are seeing in the intercept will be seen at 0dBm as well. Below, I've clipped the response of the ADL5506 which has some more detail, but you can see the relationship between the intercept/slope and the response at higher power.


    I don't have the spread for the intercept point for this part, and the ESD rating is 1.5kV HBM and 1kV CDM. 

Children