I am looking for a RF switch which can handle +28dBm maximum CW power, non-reflective, SPDT with Bandwidth of 20MHz to 25GHz.
I noticed the ADRF5031 is specified for 9kHz to 20GHZ however in the given figures if I use it up to 25ghz means that I am just accepting a larger loss at higher frequencies, which for my application is suitable.
My question is: since the part is only advertised as 9kHz to 20GHZ is there a reason why it could not be used above 20GHz which I am missing? Secondly do you have a more suitable SPDT switch for such application?