Post Go back to editing

ADL8100: About the input return loss of the datasheet

Category: Hardware
Product Number: ADL8100

Hi,

Our customer asked to me that is the input return loss of figure 17 in the datasheet of ADL8100 same as the figure 5 in the user guide of UG-2128?

Please tell me that is same as the input return loss in the datasheet and in the user guide or not.

(Certainly, I seem those are same when I compare to two input return losses.)

The customer thinks the datasheet input return loss should be de-embedded input return loss.

Best Regards,

Tomohiro

Parents Reply Children