Post Go back to editing

ADRF5024 SWITCH NOT SWITCHING TO ONE PORT TO ANOTHER

Thread Summary

The user is experiencing failures with the ADRF5024 RF switch, where it switches to RF1 but not RF2 when the CTRL signal is low. The power-up sequence and RF power levels are within specifications, and no DC values are present on the RF lines. The final answer suggests probing Vdd, Vss, and control signals with an oscilloscope to check for AMR violations and ensure proper power-up timing. The user has confirmed the power-up sequence and RF line conditions, and will provide further measurements.
AI Generated Content
Category: Hardware
Product Number: ADRF5024

Hello,

We are using the switch with part number ADRF5024 in a project, but we are having big problems while using it and so far 4 switches have unfortunately broken down and become unusable.
The way we use ADRF5024 in our circuit is as follows.

1.As stated on page 10 of the datasheet (RevD), the ideal power-up sequence is followed, first VDD 10ms and then VSS is switched on.
2.CTRL (0 to +3.3V) signal first passes through a Voltage level Translator and then through a series 1k resistor.
3.Finally RF signal is given.

However, after a while, all switches broke down and started to react as follows.
When we switch the CTRL signal to the high position (+3.3V), it switches to RF1, but when we pull it to the low position (0V), it does not switch to RF2 and behaves like in isolation.
CTRL signals are under over voltage and negative voltage protection with Voltage Level Translator. We verified that this was not the case during our tests.
Likewise, VDD and VSS voltages were also tested and verified.



What kind of problem could we be encountering in the above circuit? We ask for your urgent support in solving this problem.
Best Regards,
Adem

Parents
  • It seems there's no issue with supply sequencing and no AMR value is violated with CTRL and supply pins.

    The failures may be due to excessive RF power. Recommended power level for RFC is 27 dBm and 26 dBm if the input is at RF1 / RF2. What's the max. RF power level you work? Also verify you're not applying RF power to an unselected RF pin. 

  • Hello Yus,

    I noticed a missing part in my answer.
    Yes, we do not apply RF power to a non-working port and the maximum RF power that will come to that port is also below 0 dBm.
    I request your quick feedback in order to operate this circuit, which we urgently need, as we want.
    Best Regards,
    Adem

  • It seems RF power level is low enough to be a concern. 
    I suggest probing Vdd, Vss and Control signals near IC pins with an oscilloscope in order to make sure there's no AMR violation due to ringing or any other system related problem. Please make sure you don't apply control signal when Vdd and Vss of ADRF5024 are off. I also suggest checking Vdd and Vss power up timings with an oscilloscope probing. Please make sure Vdd is turning on before Vss.

    I'd like to remind ADRF5024's RF lines are dc-coupled to 0 V and no DC value other than 0V is recommended. You would need a DC blocking capacitor in case the RF line potential is not 0V.

  • Hello Yus,

    I checked the VDD, VSS and CTRL pins with an oscilloscope. VSS comes after VDD and the signal levels are normal.
    I also checked the RF lines and verified that there is no DC value and there is no DC signal along the line.
    Control signals come after the supply voltages.
    4 ICs have already become unusable. Do you have any idea where the problem is caused so that other integrations do not fail?
    Thank you in advance for your support
    Best Regards
    Adem

  • ADRF5024s were able to switch RF1 and to RF2 before failure at least few times, am I right? What's average failure time or switching count, can you give an approximate number?

    "When we switch the CTRL signal to the high position (+3.3V), it switches to RF1, but when we pull it to the low position (0V), it does not switch to RF2 and behaves like in isolation."

    Regarding your explanation above: Do both RF1 and RF2 stay in isolation state when you apply logic low and expect to select RF2? Or RF1 is stayed selected (insertion loss mode, showing expected loss)? 

    We hope to localize the electrically stressed location in principle. Can you measure RF pin resistance of the failed units. RFC should be around 16k and RF1/2 should be around 3.4k? The expected resistance for the other pins as follows: VSS ~18k, VDD~350k and CTRL >1 Mohm.

    Can you measure the VDD, VSS and CTRL pin currents of the failed units? It can be hard to measure this if ADRF5024 share voltage rail with other components. The most convenient way is to utilize the evaluation board if you have it already.









Reply
  • ADRF5024s were able to switch RF1 and to RF2 before failure at least few times, am I right? What's average failure time or switching count, can you give an approximate number?

    "When we switch the CTRL signal to the high position (+3.3V), it switches to RF1, but when we pull it to the low position (0V), it does not switch to RF2 and behaves like in isolation."

    Regarding your explanation above: Do both RF1 and RF2 stay in isolation state when you apply logic low and expect to select RF2? Or RF1 is stayed selected (insertion loss mode, showing expected loss)? 

    We hope to localize the electrically stressed location in principle. Can you measure RF pin resistance of the failed units. RFC should be around 16k and RF1/2 should be around 3.4k? The expected resistance for the other pins as follows: VSS ~18k, VDD~350k and CTRL >1 Mohm.

    Can you measure the VDD, VSS and CTRL pin currents of the failed units? It can be hard to measure this if ADRF5024 share voltage rail with other components. The most convenient way is to utilize the evaluation board if you have it already.









Children