Post Go back to editing

ADRF5024 SWITCH NOT SWITCHING TO ONE PORT TO ANOTHER

Thread Summary

The user is experiencing failures with the ADRF5024 RF switch, where it switches to RF1 but not RF2 when the CTRL signal is low. The power-up sequence and RF power levels are within specifications, and no DC values are present on the RF lines. The final answer suggests probing Vdd, Vss, and control signals with an oscilloscope to check for AMR violations and ensure proper power-up timing. The user has confirmed the power-up sequence and RF line conditions, and will provide further measurements.
AI Generated Content
Category: Hardware
Product Number: ADRF5024

Hello,

We are using the switch with part number ADRF5024 in a project, but we are having big problems while using it and so far 4 switches have unfortunately broken down and become unusable.
The way we use ADRF5024 in our circuit is as follows.

1.As stated on page 10 of the datasheet (RevD), the ideal power-up sequence is followed, first VDD 10ms and then VSS is switched on.
2.CTRL (0 to +3.3V) signal first passes through a Voltage level Translator and then through a series 1k resistor.
3.Finally RF signal is given.

However, after a while, all switches broke down and started to react as follows.
When we switch the CTRL signal to the high position (+3.3V), it switches to RF1, but when we pull it to the low position (0V), it does not switch to RF2 and behaves like in isolation.
CTRL signals are under over voltage and negative voltage protection with Voltage Level Translator. We verified that this was not the case during our tests.
Likewise, VDD and VSS voltages were also tested and verified.



What kind of problem could we be encountering in the above circuit? We ask for your urgent support in solving this problem.
Best Regards,
Adem

Parents
  • It seems there's no issue with supply sequencing and no AMR value is violated with CTRL and supply pins.

    The failures may be due to excessive RF power. Recommended power level for RFC is 27 dBm and 26 dBm if the input is at RF1 / RF2. What's the max. RF power level you work? Also verify you're not applying RF power to an unselected RF pin. 

  • Hello Yus,

    Our RF power input level is much lower than 27 dBm, I would say below 0 dBm. We are also sure that there is no RF power to other pins.
    However, we are still having this problem.

    Best Regards
    Adem

Reply Children
No Data