Dear Forum,
I am trying AD608 using 21.4MHz IF crystal filter (MCF) with 1.5K characteristic impedance. My problem, - it seems - the filter is somehow bypassed and I cannot achieve
the desired out-band signal rejection (~80-90dB) only ca 55dB.
If refer to datasheet Fig.23 designations.
RFHi is 50mV peak (max allowed level for 1dB compression).
if IF is exactly 21.4MHz RSSI is 1.78V ->OK.
iF no signal at input: RSSI ~0,23V->OK.
I test the out band signal rejection ("far selectivity / stopband atten") by applying a signal at RFHi producing -with oscillator frequency- a different IF then nominal 21.4M, say 20MHz.
RSSI is ~0,7V -> should be 0,23V.
If the filter is removed but R3 (1.5K) leaved RSSI is still ~0.7V ->should be 0,23V.
If R3 is shorted by 33nF RSSI is still ~0,7V
if R1 is shorted by 33nF RSSI is still ~0,7V (~very small decreasing, only minor change)
if RFHi is is shorted by 33nF RSSI now ~0,23V ->this is OK.
Offset nulling feedback loop works nicely (Voltage at IFHI and IFLO is the same within few mV error 2V VMID).
Supply is bypassed using 1uF Tantal + 3.3nF C0G. C5 10nF X7R, C1 was chaged from 22nF X7R to 100nF but any results.
I tried to change R4 from 100R to 1K but not improvement.
I would be happy if somebody could give advise to eliminate the coupling isse.
Thanks:
Joseph