Post Go back to editing

JESD204B link

Category: Datasheet/Specs
Product Number: ad9375

Hi,

The current frequency on our JESD204B is configured at 44 Msps. We would like to reduce it to 22 Msps, which seems compatible according to the data sheet. However, we are facing a limitation imposed by the configuration wizard. The AD9375 wizard restricts the Tx frequency to 30 Msps and the Rx frequency to 20 Msps.

In our setup, we are unable to operate with two different frequencies on a single link, so both Rx and Tx would need to be at 22 Msps.

Is this limitation coming from the AD9375 itself, or is it just due to the wizard? Can we bypass the wizard for Tx mode? Additionally, we want to clarify that we do not plan to use DPD, assuming that the Tx limitations are related to DPD.

thanks.

Damien

Parents Reply
  • 614.4Mbps * 8/10 / 32 = 15.36Msps.
    Why the sample rates is not limited to 15.36MSPS?
    Why the wizard limit to 30MSPS in TX and 20MSPS in RX?

    In TX the wizard limit is 30MSPS, so JESD data rate = 1200 Mbps

    In RX the wizard limit is 20MSPS, so JESD data rate = 800 Mbps

    both wizard limit are far from 614.4Mbps

Children
No Data