Hi to all!
For this Power Switch there is the following specification about switching speed:
Rise and Fall time (10% to 90% of RF output): 200ns typ.
According to this performance, it seems to me that a pulsed signal at the input with very steep edges can be distorted. On the other hand, this switch is wideband and ensures a very good linearity, being 0.1dB Compression Point as high as 50dBm. Therefore it seems that Rise/fall time and linearity performance are not coherent. Where am I wrong?
I would like to use this switch for a TX/RX application but I guess that it is not the best solution for its performance in terms of Rise/Fall Time and RF Settling Time (1.2us). Any suggestion about a possible alternative?
Thanks in advance.
Giuliano