I have four AD8307 log detectors on a board. I am seeing considerable crosstalk between them. For example, if I feed any one of them with -20dBm at 144MHz, its output rises from quiescent 0.25V to ~1.8V as it should but the others rise to 0.5-0.9V. The devices closer to the receiving device are affected more than the ones farther away.
The board is 4-layer: Top analog signal, continuous copper ground plane, digital, and power. The devices are separated by about 2cm and their outputs feed an ADC. The crosstalk is unrelated to the ADC because it happens even if the ADC is unsoldered.
Is this behavior normal? Do I need to shield the devices from each other?
Thanks