Post Go back to editing

ADF5901 output power

Category: Datasheet/Specs
Product Number: ADF5901

Hello, I would like to ask whether the output power adjustment of the ADF5901 is controlled through Register 1, specifically DB12~DB5? Does 0 correspond to -20dBm and 255 correspond to 8dBm? Is the adjustment evenly spaced? If I want to set the output power to around 0dBm, should I set it to approximately 183?

I plan to connect a power amplifier (PA), the HMC863ALC4, to the output. This amplifier has a gain of 24dB and a P1dB output of 27dB. Therefore, setting the ADF5901 output to 0dBm seems more appropriate. Would this approach be feasible?

Additionally, do I need to adjust the AUX BUFFER GAIN in the ADF5901? What is its function?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.