KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC5589
Production
The LTC5589 is a direct conversion I/Q modulator designed for low power wireless applications that enables direct modulation of differential baseband I...
Datasheet
LTC5589 on Analog.com
LTC5598
Last Time Buy
The LTC5598 is a direct I/Q modulator designed for high performance wireless applications, including wireless infrastructure. It allows direct modulation...
Datasheet
LTC5598 on Analog.com
Hello all,
Regarding LTC5589 I/Q input DC bias,
There is an internally generated 1.4V DC bias.
Q1: The datasheet mentions an option to disable the internal bias. How can this be achieved?

Q2: I am using an FDA with a common-mode voltage of 1.65V. What would happen if I connect 1.65V-biased I/Q signals to the modulator inputs? My assumption is that it should be fine due to the 1kΩ resistors between the input and the internal reference, but I would like to confirm.
Thanks
Nir
Hi Nir, I did not see a reference in the datasheet to disabling the internal bias voltage. It does however state that the external bias voltage should not exceed "2 x Vdc" where Vdc is 1.4 V. So that says that there will be no problem with applying an external dc bias voltage of 1.65V
Hi Enash,
I couldn’t find any reference either. I assume this switch only indicates that the bias can be disabled, perhaps when the device is powered off (EN = 0).
Regarding biasing at 1.65V—yes, I looked at this note just today. I’ll verify that it's okay using the evaluation board.
Thanks for helping!
Nir